How to develop Smart meter application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to develop Smart meter application

1,432 Views
arun_bhardwaj21
Contributor I

I am very new for these kind of programming. I am trying to create a Smart meter application. I want to create an application, which will collect data from installed meters, which are located at different locations. And I can create different report. The application can also send signal to meter to on/off the meter.

My Questions: I have work experience in Java for web-development. Just to save time, I want to understand-

From where I should start? which IDE is suitable to develop this app?

Any Mock/simulator, which can be used as a meter?

Which software packages on NXP or anywhere, I should look first?

Any other suggestion or link, which I can refer.

Thanks in advance for your help.

0 Kudos
Reply
1 Reply

1,384 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Arun Bhardwaj

  If you want to design the meter, you can check the kinetis KM series:

Arm® Cortex®-M0+|Kinetis® KM3x 50-75 MHz 32-bit MCUs | NXP 

  There some designs for your reference.

  Please check it at first, you will find the related IDE, software.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply