How to create project for S9KEAZN32AMLC microcontroller in Codewarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to create project for S9KEAZN32AMLC microcontroller in Codewarrior

ソリューションへジャンプ
2,206件の閲覧回数
rkavinash03
Contributor I

How to create project for S9KEAZN32AMLC microcontroller in codewarrior. ??

ラベル(1)
0 件の賞賛
返信
1 解決策
2,187件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi rkavinash03,

Sorry for the inconvenience we bring you!
This is a known issue of ProcessorExpert of CodeWarrior. You may select MKE02Z32xxx4 PEx cpu component. Or use KDS3.2 instead of CodeWarrior.

Note the trimming. The KEAZN32 and KE02Z32 devices ship from the factory with factory trim to 32MHz. To get the part operating at 40MHz requires the internal clock source ICS to have *user* trim (to 39.0625 kHz (upper limit)). Normally this user trim is written into flash at 0x0000_03FF/03FE and must be copied into the ICS_C3 register by the startup code. Simply setting the PEx CPU component ‘Slow internal reference clock [kHz]’ to 39.0625 does not make the clock 40MHz. 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,188件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi rkavinash03,

Sorry for the inconvenience we bring you!
This is a known issue of ProcessorExpert of CodeWarrior. You may select MKE02Z32xxx4 PEx cpu component. Or use KDS3.2 instead of CodeWarrior.

Note the trimming. The KEAZN32 and KE02Z32 devices ship from the factory with factory trim to 32MHz. To get the part operating at 40MHz requires the internal clock source ICS to have *user* trim (to 39.0625 kHz (upper limit)). Normally this user trim is written into flash at 0x0000_03FF/03FE and must be copied into the ICS_C3 register by the startup code. Simply setting the PEx CPU component ‘Slow internal reference clock [kHz]’ to 39.0625 does not make the clock 40MHz. 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信