How to connect PN7462 with FRDM K64F as a master?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to connect PN7462 with FRDM K64F as a master?

1,168 次查看
nidhintomy
Contributor IV

How to connect PN7462 with FRDM K64F as a master?

Is PN7462 is standalone to drive motors,light led?

0 项奖励
回复
2 回复数

1,120 次查看
nidhintomy
Contributor IV

Thanks

0 项奖励
回复

1,162 次查看
bobpaddock
Senior Contributor III

What is the actual task that needs solved?

The PN7462 can be connected to K64F as UART.

It will not drive a motor directly.
It lacks the required drive current.
NFC may also have more time lag that is allowed in motor control (the actual task matters).

It may be able to drive LEDs directly, depending on the LED color and current, again the actual task matters.

The more details in a question, the more details that can be given in an answer.