How to connect PN7462 with FRDM K64F as a master?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to connect PN7462 with FRDM K64F as a master?

1,224 Views
nidhintomy
Contributor IV

How to connect PN7462 with FRDM K64F as a master?

Is PN7462 is standalone to drive motors,light led?

0 Kudos
Reply
2 Replies

1,176 Views
nidhintomy
Contributor IV

Thanks

0 Kudos
Reply

1,218 Views
bobpaddock
Senior Contributor III

What is the actual task that needs solved?

The PN7462 can be connected to K64F as UART.

It will not drive a motor directly.
It lacks the required drive current.
NFC may also have more time lag that is allowed in motor control (the actual task matters).

It may be able to drive LEDs directly, depending on the LED color and current, again the actual task matters.

The more details in a question, the more details that can be given in an answer.