How to check which interrupt has fired now?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to check which interrupt has fired now?

1,386件の閲覧回数
vikranthnk
Contributor I

I am using both receive and transmit interrupts, but in my code interrupt handler is only one for both receive and transmit is it right?

Iam using FRDMKE04 dev board,    and    SDK_2.3.1_FRDM-KE04Z

following is my sample code 

#include "board.h"
#include "fsl_uart.h"
#include "pin_mux.h"

void UART0_IRQHandler(void)
{

   if(receive interrupt)  ///// I need to know this condition

   {
      uint8_t data;
      /* If new data arrived. */
      if ((kUART_RxDataRegFullFlag | kUART_RxOverrunFlag) & UART_GetStatusFlags(UART0))
      {
            data = UART_ReadByte(UART0);
            // Copy the byte into the local FIFO, if it won't cause an overflow
            if(UART_RxBuffer_WritePtr < EUSART_RX_BUFFER_SIZE)
               {
                  UART_RxBuffer[UART_RxBuffer_WritePtr++] = data;

                  if(UART_RxBuffer_WritePtr >= EUSART_RX_BUFFER_SIZE)
               {
                     UART_RxBuffer_WritePtr = 0;
         }

                  UART_NumBytesInRxBuffer++; /* Update counter */
   }

   elseif(transimit interrupt is fired) ///// I need to know this condition

   {


   }

}

0 件の賞賛
返信
1 返信

1,269件の閲覧回数
mjbcswitzerland
Specialist V

Hi Vikranth

You need to read UART0_S1 to see which interrupt flag is set [UART_S1_TDRE, UART_S1_RDRF, or both].

Regards

Mark


uTasker developer and supporter (+5'000 hours experience on +60 Kinetis derivatives in +80 product developments)

Kinetis: http://www.utasker.com/kinetis.html
Kinetis KE:
- http://www.utasker.com/kinetis/FRDM-KE02Z.html
- http://www.utasker.com/kinetis/FRDM-KE02Z40M.html
- http://www.utasker.com/kinetis/FRDM-KE04Z.html
- http://www.utasker.com/kinetis/FRDM-KE06Z.html
- http://www.utasker.com/kinetis/FRDM-KE15Z.html
HW Timers: http://www.utasker.com/docs/uTasker/uTaskerHWTimers.PDF

Free Open Source solution: https://github.com/uTasker/uTasker-Kinetis
Working project in 15 minutes video: https://youtu.be/K8ScSgpgQ6M

For better, faster, cheaper product developments consider the uTasker developer's version, professional Kinetis support, one-on-one training and complete fast-track project solutions to set you apart from the herd : http://www.utasker.com/support.html

0 件の賞賛
返信