How to calibrate the dac on KL25z?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to calibrate the dac on KL25z?

914 Views
royal_agha
Contributor I

is there an automatic calibration function for the DAC? I know there is a calibration function for the ADC where the processor calculates the necessary calibration values. Is there something similar for the DAC? if not what is the best way to calibrate it especially with the non-linear behavior at very low voltage outputs(0.02 volts is the lowest I need )?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

764 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Royal,

For the better performance of DAC, I'd like to suggest refer for design as below to improve the bandwidth preformance.

And please place this capacitance as close as the corresponding DACx_OUT pin as possible on the layout.

Untitled.jpg

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply