How to byte program SPI flash via QSPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to byte program SPI flash via QSPI

How to byte program SPI flash via QSPI

How to byte program SPI flash via QSPI

QSPI module are used in many Kinetis MCU, like K8x, K27/28 and KL8x. QSPI expands the internal flash range and can run in a fast speed. Compared to DSPI, QSPI is very complex and often takes a lot of time to learn. In KSDK there are two QSPI demo which shows how to program SPI flash in DMA mode and polling mode. Both of them program the QSPI flash with a word type array. But can the QSPI module program SPI Flash in byte? Yes, this article shows how to do it.

Device: FRDM_KL82Z

Tool: MCUXpresso IDE

Debug firmware: JLINK

I build the test project base on KL82 SDK/driver_example/qspi/polling_transfer. To byte program SPI flash, a new LUT item must be added.

uint32_t lut[FSL_FEATURE_QSPI_LUT_DEPTH] =

   {/* Seq0 :Quad Read */

         /* CMD:       0xEB - Quad Read, Single pad */

         /* ADDR:       0x18 - 24bit address, Quad pads */

         /* DUMMY:     0x06 - 6 clock cyles, Quad pads */

         /* READ:       0x80 - Read 128 bytes, Quad pads */

       …

       …

       [32] = QSPI_LUT_SEQ(QSPI_CMD, QSPI_PAD_1, 0x02, QSPI_ADDR, QSPI_PAD_1, 0x18),

       [13] = QSPI_LUT_SEQ(QSPI_WRITE, QSPI_PAD_1, 0x1, 0, 0, 0),

       …

       /* Match MISRA rule */

       [63] = 0};

This item tells system how to program a single byte.

Then when we write the data to TxBuffer, we must write the byte 4 times. This is because a write transaction on the flash with data size of less than 32 bits will lead to the removal of four data entry from Txbuffer. The valid bit will be used and the rest of the bits will be discard.

Then before we start programming, we must set the data size.

     QSPI_SetIPCommandSize(EXAMPLE_QSPI,1);

 

After byte program, we can see the result from 0x68000000.

205845_205845.pngqspi_byte_program.png

Attachment is the demo project. You can find that 0x03 was written to 0x68000005 after running.

添付
評価なし
バージョン履歴
最終更新日:
‎12-11-2017 08:19 PM
更新者: