How to attach source file path to existing project in code warrior v10.6 (Micro controller based)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to attach source file path to existing project in code warrior v10.6 (Micro controller based)

4,464件の閲覧回数
communitycommun
Contributor III

Hello

               I am trying to add the source file path to the existing project in the project explore window in code warrior v10.6.Since very new to this eclipse based IDE provide my NXP.

It would be very helpful if some one could help me up about this ...

Thanking you

0 件の賞賛
返信
3 返答(返信)

4,330件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

Please right click your project ,then select properties , then refer to the picture to add source file path :

pastedImage_0.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,330件の閲覧回数
communitycommun
Contributor III

Thanks Alice_Yang

                                  i have done exactly what you said,but in my IDE there is no folder named directives instead input is given with the same picture..i have attached below........

so does both are same..i believe it's same but still need confirmation.....

Thanks Alice_Yang

0 件の賞賛
返信

4,330件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

Sorry i have not see any picture .

Please send it again , and  also i recommend you send your project and

point out the file to me , i also can test it on my side .

BR

Alice

0 件の賞賛
返信