How to allocate KW38 freedom bootloaderand BLE application storage area?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to allocate KW38 freedom bootloaderand BLE application storage area?

Jump to solution
2,852 Views
wenhuafeng
Contributor II

Hi everyone,

I use MCUXpresso IDE (V11.2.1) to develop the function of KW38, and use feedom bootloader to boot the BLE application through the UART upgrade of KinetisFlashTool.exe tool, but I don’t know how to allocate the FALSH and RAM space of the BLE application to correspond to the FLASH of the feedom bootloader , RAM space can be upgraded by this method?

 

Freedom bootloader FLASH and RAM space are as follows:

1.jpg

BLE wireless_uart_bm FLASH and RAM space are as follows:

2.jpg

The names of FLASH and RAM, FEFT_2K.cfx, FEFT_2K_D.cfx, do not know what they mean, is there any relevant documentation?

"MCU Bootloader Demo Application User's Guide.pdf", I tried the examples inside, and it can be programmed normally as described in the document.

thank you very much!

0 Kudos
Reply
1 Solution
2,803 Views
nxf56274
NXP Employee
NXP Employee

Hi,

You do not modify the application's size. 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
2,826 Views
nxf56274
NXP Employee
NXP Employee

Hi,

If your bootloader will go to address 0xa000, you can configure like this.

You should modify the application's Location and the size.

4.PNG

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,806 Views
wenhuafeng
Contributor II

Hi,TIC

Modify here, there is an error message!

1.JPG

0 Kudos
Reply
2,804 Views
nxf56274
NXP Employee
NXP Employee

Hi,

You do not modify the application's size. 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply