How to access PTA2 and PTA3 pins for I2C communication on FRDM-KE02Z board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to access PTA2 and PTA3 pins for I2C communication on FRDM-KE02Z board?

1,716 Views
mstagg
Contributor I

The board uses PTA2 and PTA3 for I2C communications, but both of these pins are already used by the on-board accelerometer. PTB6 and PTB7 are the other options, but they are running an on-board clock. How can I use I2C communication on this board if all the allocated pins are already used by on-board components?

Please don't yell at me. I'm an intern.

Tags (3)
2 Replies

1,492 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Matthew Stagg,

      

Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,492 Views
mjbcswitzerland
Specialist V

Hi Matthew

I2C is a bus that can have many devices on it so the fact that the accelerometer is connected to PA2 and PA3 don't restrict you from using the same bus lines for furter devices with difference addresses.

Regards

Mark

Kinetis: µTasker Kinetis support

KE: µTasker FRDM-KE02Z support  / µTasker FRDM-KE02Z40M support  / µTasker FRDM-KE06Z support

For the complete "out-of-the-box" Kinetis experience and faster time to market