How to Create ".SREC" Output file in Codewarriors 10.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Create ".SREC" Output file in Codewarriors 10.3

ソリューションへジャンプ
6,076件の閲覧回数
ashokra
Contributor II

Hi Iam new to Freescale and working with Kinetis Controller. I brought Freedom Development Kit and i installed code warriors v10.3.

I downloaded FRDM-KL25Z Quick Start Package In that i could see some precompiled example (i.e "*****.srec" output files ) but I am not able to create ".srec" output file with codewarriors. i just want to develop simple LED blinking project can anyone help me?

ラベル(1)
タグ(1)
1 解決策
2,731件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

- How to generate SREC (or S19) file: S-Record Generation with gcc for ARM/Kinetis | MCU on Eclipse

- LED's with the Freedom board: Tutorial: Enlightning the Freedom KL25Z Board | MCU on Eclipse

- Other things for the Freedom board: KL25Z Freedom Board | MCU on Eclipse

Hope this helps.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,731件の閲覧回数
ashokra
Contributor II

Thank you!  Erich , its very useful.... :-)

0 件の賞賛
返信
2,731件の閲覧回数
SriViswatej_R_v
Contributor I

Hello ,

I'm new to free scale FRDM KL25 board.

I installed code warrior 10.5.

I downloaded the sample code.

I have seen the Quickstart package.

The pre-compiled code works well in the board.

But i'm unable to dump anything in the board. I want to dump the sample code in to it.

Please tell me the procedure to dump the coding into the board.

If possible please give me the link for reference.

Thank you.

0 件の賞賛
返信
2,732件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

- How to generate SREC (or S19) file: S-Record Generation with gcc for ARM/Kinetis | MCU on Eclipse

- LED's with the Freedom board: Tutorial: Enlightning the Freedom KL25Z Board | MCU on Eclipse

- Other things for the Freedom board: KL25Z Freedom Board | MCU on Eclipse

Hope this helps.

0 件の賞賛
返信