How many clk will DMA take to complete ADC data transmission

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How many clk will DMA take to complete ADC data transmission

ソリューションへジャンプ
2,114件の閲覧回数
王剑翰
Contributor III

For K10, if I use ADC to capture data and DMA to translate the data, how many clk will DMA take to complete ADC data transmission?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,049件の閲覧回数
EarlOrlando
Senior Contributor II

Sorry I didn't notice that you specified that you are using the K10 MCU but I took a look into the K10 reference manual and the EDMA peripheral is exactly the same so the information that I provided is correct.

Best regards,

Earl.

元の投稿で解決策を見る

3 返答(返信)
2,049件の閲覧回数
EarlOrlando
Senior Contributor II

Hello,

The DMA performance is reported in the reference manual. I.e. for the K64F in its reference manual in the chapter 22.4.4 is documented how to calculate the time that the DMA needs to complete a transaction. In this case the transaction corresponds to a an internal peripheral to internal SRAM so it needs 9 clock cycles assuming zero wait-states. For a more detailed information please go to the reference manual.

Best regards,

Earl.

2,050件の閲覧回数
EarlOrlando
Senior Contributor II

Sorry I didn't notice that you specified that you are using the K10 MCU but I took a look into the K10 reference manual and the EDMA peripheral is exactly the same so the information that I provided is correct.

Best regards,

Earl.

2,049件の閲覧回数
王剑翰
Contributor III

Hi Earl,

Sorry for late, and thanks for your kindly reply!

I have checked it.

0 件の賞賛
返信