How do you access the persistent memory/non volatile area in 22F?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do you access the persistent memory/non volatile area in 22F?

1,533件の閲覧回数
cwati
Contributor III


Is there an existing way, or readily available API in the K22F bare metal code that comes with the basic demos, to read/write into persistent memory? (So the values are stored across reboot).

Specifically, we're using MK22FN256xxx12, so it's not quite the Freedom board since it has less flash.

Thanks,
Cecylia

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,318件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Cecylia,

I'd highly recommend you to use the stand software driver which consist of a set of APIs, and the stand software driver for the C90TFS/FTFx flash will provide driver functions to perform high-speed program/erase operation.

Please go for download the driver through the link as below, it also has some demo for referring to.

http://cache.freescale.com/files/32bit/software/C90TFS_FLASH_DRIVER.exe?fromsite=zh-Hans
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,318件の閲覧回数
cwati
Contributor III

Thank you! We'll give it a try.

0 件の賞賛
返信