How do the on chip True Random Number Generators work?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How do the on chip True Random Number Generators work?

跳至解决方案
4,088 次查看
bobpaddock
Senior Contributor IV

Several NXP chips have added True Random Number Generators.

I really would like to see some data from NXP on how it works and what NIST tests its has passed.

I know what some places do is take a mediocre noise source and run it through a hash algorithm to make it appear better than it truly is. 

Any true random process will also make a really good thermometer.


Take a look at the Random Number section:

https://www.schneier.com/academic/

 

0 项奖励
回复
1 解答
4,066 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @bobpaddock ,

TRNG is based on collecting bits from a random noise source. This random noise source is a ring oscillator that is sensitive to random noise (temperature variations, voltage variations, cross-talk and other random noise) within the device in which the TRNG is used. TRNG can be used to seed a hardware or software based implementation of a DRBG defined by SP800-90.

TRNG hasn't been certified with FIPS and there are no plans to do it for KINETIS.

But, the TRNG is designed in accordance with SP800-90B guidelines, if you combine it with a SW DRBG (per SP800-90B guidelines), it should meet the FIPS requirements.

 

Regards,

Jing

在原帖中查看解决方案

0 项奖励
回复
2 回复数
4,067 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @bobpaddock ,

TRNG is based on collecting bits from a random noise source. This random noise source is a ring oscillator that is sensitive to random noise (temperature variations, voltage variations, cross-talk and other random noise) within the device in which the TRNG is used. TRNG can be used to seed a hardware or software based implementation of a DRBG defined by SP800-90.

TRNG hasn't been certified with FIPS and there are no plans to do it for KINETIS.

But, the TRNG is designed in accordance with SP800-90B guidelines, if you combine it with a SW DRBG (per SP800-90B guidelines), it should meet the FIPS requirements.

 

Regards,

Jing

0 项奖励
回复
4,061 次查看
bobpaddock
Senior Contributor IV

Thank you.

0 项奖励
回复