How do I flash .out or .afx files?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How do I flash .out or .afx files?

跳至解决方案
1,923 次查看
anguel
Contributor V

Hi!

I found some precompiled demos for the TWR-K70F120M and the TWR-LCD-RGB here:

TWR-LCD-RGB Product Summary Page

These are .out files (from IAR) and .afx files (form CodeWarrior). I wonder if I can flash those files with the free versions of those IDEs or with some other tools to be able to see the demos?

Thanks,

Anguel

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
1,478 次查看
BlackNight
NXP Employee
NXP Employee

There are several way to flash files of any size with CodeWarrior:

Using command line tools:

Standalone Flash Programmer | MCU on Eclipse

Using the 'Flash' button:

Flashing with a Button | MCU on Eclipse

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,479 次查看
BlackNight
NXP Employee
NXP Employee

There are several way to flash files of any size with CodeWarrior:

Using command line tools:

Standalone Flash Programmer | MCU on Eclipse

Using the 'Flash' button:

Flashing with a Button | MCU on Eclipse

0 项奖励
回复
1,478 次查看
anguel
Contributor V

Erich,

Thank you. I will try this as soon as I have the hardware.

Actually I looked at the flash tool in CodeWarrior but was confused because it asked for some flash configuration file and I only have a single .afx file in the demos.

Regards,

Anguel

0 项奖励
回复
1,478 次查看
anguel
Contributor V

Thank you once again Erich!

I tried your second tutorial and it worked fine.

Regards,

Anguel

0 项奖励
回复