How do I flash .out or .afx files?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I flash .out or .afx files?

ソリューションへジャンプ
2,717件の閲覧回数
anguel
Contributor V

Hi!

I found some precompiled demos for the TWR-K70F120M and the TWR-LCD-RGB here:

TWR-LCD-RGB Product Summary Page

These are .out files (from IAR) and .afx files (form CodeWarrior). I wonder if I can flash those files with the free versions of those IDEs or with some other tools to be able to see the demos?

Thanks,

Anguel

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,272件の閲覧回数
BlackNight
NXP Employee
NXP Employee

There are several way to flash files of any size with CodeWarrior:

Using command line tools:

Standalone Flash Programmer | MCU on Eclipse

Using the 'Flash' button:

Flashing with a Button | MCU on Eclipse

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,273件の閲覧回数
BlackNight
NXP Employee
NXP Employee

There are several way to flash files of any size with CodeWarrior:

Using command line tools:

Standalone Flash Programmer | MCU on Eclipse

Using the 'Flash' button:

Flashing with a Button | MCU on Eclipse

0 件の賞賛
返信
2,272件の閲覧回数
anguel
Contributor V

Erich,

Thank you. I will try this as soon as I have the hardware.

Actually I looked at the flash tool in CodeWarrior but was confused because it asked for some flash configuration file and I only have a single .afx file in the demos.

Regards,

Anguel

0 件の賞賛
返信
2,272件の閲覧回数
anguel
Contributor V

Thank you once again Erich!

I tried your second tutorial and it worked fine.

Regards,

Anguel

0 件の賞賛
返信