How can J-Flash flashing MKE06Z128VLK4?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can J-Flash flashing MKE06Z128VLK4?

1,631 Views
matherinewang
Contributor III

Hi Friends,

I prepare use SEGGER J-Flash for MKE06Z128VLK4.

But when i execute File->Open Project, i find there are many *.jflash files here but seems no one for MKE06Z128VLK4.

how can i flash MKE06Z128VLK4 with J-Flash? is it means i can't do it? Thanks in advance

Labels (1)
0 Kudos
Reply
1 Reply

1,262 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi matherine wang,

You can use “Create a new project” instead of "Create project from template".

Just refer to the following step:

1: Create a new project

53.jpg

2: do Project settings

54.jpg

3: Select KE06Z128VLK4, Then save the .jflash, this is what you needed.

pastedImage_0.png

Wish it helps your.

If you still have question, please contact me!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply