How can I set the MKL02Z to 48MHZ using FEI.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can I set the MKL02Z to 48MHZ using FEI.

2,971 次查看
clivepalmer
Contributor III

Hi,

I am trying to set my MKL02Z16 to run at 48MHZ using the internal clock (FEI mode). I had written the code manually and had set MCG_C4 to have DRST_DRS to MID range  (01) and DMX32 to 1. Looking a the register description it suggested that this would give a FLL factor of 1464 and using the slow refrerence clock of 32.768KHZ I would get a DCO of approx. 48MHZ, and hence a MCGFLLCLK of 48MHZ.

I have just run through an exercise on processor expert to check my settings and although it will allow me to set a FLL factor of 1464 and does shows the correct 48MHZ frequency. It tells me it is not possible to set the requested value in the Problems Eclipse warning panel. This puzzles me. What have I overlooked or done wrong? How do I get 48MHz or is this not possible on the KL02 part?

I need to resolve this as all my peripheral clock have been set based upon a MCGFLLCLK of 48MHZ.

Thanks.

Clive

标签 (1)
0 项奖励
回复
4 回复数

1,892 次查看
clivepalmer
Contributor III

Thank you both for taking the time to reply. I had written the code from the RM, but then installed Processor Expert 10_4. I am using GNU tools and Eclipse.

I'm relived to know it is possible but now confused as to why it will not allow me to set it in PE. If it wont set it correctly in PE then I cant set the clocks correct for my peripheral.

0 项奖励
回复

1,892 次查看
Derrick
NXP Employee
NXP Employee

Hi Clive,

I suggest comparing your Processor Expert screen to mine (from CodeWarrior v10.6).  There may be something slightly different.  As I state, I don't get an error.

The only changes that I made from the default configuration were:

1) change Clock settings > Clock source settings > Clock source setting 0 > MCG settings > FLL settings > FLL output (MHz)  to  "48"  - which gets translated to "47.972352"

2) change Clock configurations > Clock configuration 0 > System clocks > Core clock  to  "48"  - which gets translated to "47.972352"

3) change Clock configurations > Clock configuration 0 > System clocks > Bus clock  to  "24"  - which gets translated to "23.986176"

When using the stand alone Processor Expert Software Microcontroller Driver Suite v10.4, these frequency changes are made via drop down menus.  Here are the corresponding screen shots, with the changes highlighted, first under the "Properties" tab:

pastedImage_0.png

Then under the "Clock configurations" tab:

pastedImage_1.png

Selecting the frequencies from the menus shouldn't generate any sort of error.

Best Regards,

Derrick

0 项奖励
回复

1,892 次查看
Derrick
NXP Employee
NXP Employee

Hi Clive,

Are you using Processor Expert from within CodeWarrior or the separate tool?  Current versions are:

- CodeWarrior for Microcontrollers v10.6 (with Processor Expert integrated within)

- Processor Expert Software, Microcontroller Driver Suite v10.4 (stand alone tool version)

I checked both of these and I do not see the error which you mention.  Both generate the same code:

  /* System clock initialization */

  /* SIM_CLKDIV1: OUTDIV1=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,OUTDIV4=3,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */

  SIM_CLKDIV1 = (SIM_CLKDIV1_OUTDIV1(0x00) | SIM_CLKDIV1_OUTDIV4(0x03)); /* Set the system prescalers to safe value */

  /* SIM_SCGC5: PORTB=1,PORTA=1 */

  SIM_SCGC5 |= (SIM_SCGC5_PORTB_MASK | SIM_SCGC5_PORTA_MASK); /* Enable clock gate for ports to enable pin routing */

  if ((PMC_REGSC & PMC_REGSC_ACKISO_MASK) != 0x0U) {

    /* PMC_REGSC: ACKISO=1 */

    PMC_REGSC |= PMC_REGSC_ACKISO_MASK; /* Release IO pads after wakeup from VLLS mode. */

  }

  /* SIM_CLKDIV1: OUTDIV1=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,OUTDIV4=1,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */

  SIM_CLKDIV1 = (SIM_CLKDIV1_OUTDIV1(0x00) | SIM_CLKDIV1_OUTDIV4(0x01)); /* Update system prescalers */

  /* SIM_SOPT2: TPMSRC=1 */

  SIM_SOPT2 = (uint32_t)((SIM_SOPT2 & (uint32_t)~(uint32_t)(

               SIM_SOPT2_TPMSRC(0x02)

              )) | (uint32_t)(

               SIM_SOPT2_TPMSRC(0x01)

              ));                      /* Set the TPM clock */

  /* Switch to FEI Mode */

  /* MCG_C1: CLKS=0,FRDIV=0,IREFS=1,IRCLKEN=1,IREFSTEN=0 */

  MCG_C1 = MCG_C1_CLKS(0x00) |

           MCG_C1_FRDIV(0x00) |

           MCG_C1_IREFS_MASK |

           MCG_C1_IRCLKEN_MASK;

  /* MCG_C2: LOCRE0=0,RANGE0=0,HGO0=0,EREFS0=0,LP=0,IRCS=0 */

  MCG_C2 &= (uint8_t)~(uint8_t)(

             MCG_C2_LOCRE0_MASK |

             MCG_C2_RANGE0(0x03) |

             MCG_C2_HGO0_MASK |

             MCG_C2_EREFS0_MASK |

             MCG_C2_LP_MASK |

             MCG_C2_IRCS_MASK

            );

  /* MCG_C4: DMX32=1,DRST_DRS=1 */

  MCG_C4 = (uint8_t)((MCG_C4 & (uint8_t)~(uint8_t)(

            MCG_C4_DRST_DRS(0x02)

           )) | (uint8_t)(

            MCG_C4_DMX32_MASK |

            MCG_C4_DRST_DRS(0x01)

           ));

  /* OSC0_CR: ERCLKEN=1,??=0,EREFSTEN=0,??=0,SC2P=0,SC4P=0,SC8P=0,SC16P=0 */

  OSC0_CR = OSC_CR_ERCLKEN_MASK;

  while((MCG_S & MCG_S_IREFST_MASK) == 0x00U) { /* Check that the source of the FLL reference clock is the internal reference clock. */

  }

  while((MCG_S & 0x0CU) != 0x00U) {   /* Wait until output of the FLL is selected */

  }

Keep in mind that the maximum bus frequency is 24MHz.  Here is how I configured this in CodeWarrior:

pastedImage_21.png

Best Regards,

Derrick

0 项奖励
回复

1,892 次查看
mjbcswitzerland
Specialist V

Clive

To set the KL02 clock to 48MHz the uTasker project does this:

OSC_CR = 0xa0

MCG_CR = 0x84

- wait for crystal source to be selected

SIM_CLKDIV1 = 0x00010000

MCG_C4 = 0xa0         // FLL factor 1464

MCG_C1 = 0

- wait until FLL source becomes valid

- wait until FLL cource is no longer the internal clock

When the external 32kHz ocillator is not used the same FLL settings are valid - but the range of the frequency tolerance is quite large.

This works reliably and the uTasker simulator checks that no values are out of range, so 1464 should not be an issue.

Regards

Mark

0 项奖励
回复