How can I set/change ADC data rate in QN9080?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How can I set/change ADC data rate in QN9080?

跳至解决方案
2,967 次查看
smittal2
Contributor III

I'm using QN9080 to develop an application. My application requires the usage of ADC to output at 400Hz. Where can I set this data rate?

Is this same as ADC down sample rate in ADC_SDDefaultConfig(), or kADC_DownSample256?

标记 (3)
1 解答
2,597 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Sandeep Mittal,

If you want to use the ADC with a sample frequency, you need to set up a timer with this frequency. In the SDK example the trigger is using the function: ADC_DoSoftwareTrigger. For you're aplication you will need to change it for a timer trigger.

You can use the adc interrupt driver example in the SDK and change the source of the trigger, in this case I'm using the CTIMER3_OUT2:

pastedImage_3.png

You'll need to set up this timer, so I suggest to you to check the ctimer simple match driver example. For the 400Hz frequency, you'll need to change the match value, the following configuration should do it:

pastedImage_4.png

Hope it helps,

Alexis Andalon

在原帖中查看解决方案

6 回复数
2,598 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Sandeep Mittal,

If you want to use the ADC with a sample frequency, you need to set up a timer with this frequency. In the SDK example the trigger is using the function: ADC_DoSoftwareTrigger. For you're aplication you will need to change it for a timer trigger.

You can use the adc interrupt driver example in the SDK and change the source of the trigger, in this case I'm using the CTIMER3_OUT2:

pastedImage_3.png

You'll need to set up this timer, so I suggest to you to check the ctimer simple match driver example. For the 400Hz frequency, you'll need to change the match value, the following configuration should do it:

pastedImage_4.png

Hope it helps,

Alexis Andalon

2,597 次查看
smittal2
Contributor III

Hi nxf46116,

Shouldn't the matchConfig.enableInterrupt be true since the ADC is triggered by ctimer?

Is BUS_CLK_FREQ 32KHz or 32MHz?

Thanks,

Sandeep

0 项奖励
回复
2,597 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Sandeep Mittal,

   

In this case I didn't enable the interrupt for the CTimer, only the ADC one. The ADC trigger is configured in the structure and this is enough to link the ADC with the CTimer. In case you want to call the CTimer Callback you should change that register.

BUS_CLK_FREQ is the APB bus clock = 16MHz

Best Regards,

Alexis Andalon

2,597 次查看
smittal2
Contributor III

nxf46116‌,

So the matchConfig.matchvalue in the data structure for ctimer will need to be BUS_CLK_FREQ/40000 to get a frequency of 400Hz, correct?

Thanks,

Sandeep

0 项奖励
回复
2,597 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Sandeep Mittal,

Have in count that the matchValue is the value where the counter is gonna trigger the interruption. Doesn't really matter what is your Bus Clock, if you divide it by the desired frequency that should work.

Best Regards,

Alexis Andalon

2,596 次查看
smittal2
Contributor III

Ok, got it. Thanks a lot for your help Alexis.

- Sandeep

0 项奖励
回复