How can I connect the DEVKIT-ZVL128 to Freemaster?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I connect the DEVKIT-ZVL128 to Freemaster?

ソリューションへジャンプ
2,671件の閲覧回数
efrain_castro
Contributor II

When i open the .pmp program that opens Freemaster and then i press the GO! icon a window appears telling me that the DEVKIT-ZVL128 is not connected then i press the Use Wizard so i can configure the connection, i choose the 

Use direct connection to on-board USB port then when choosing baud rate i choose 9600 and 115200 so it can connect but another windows appears saying No board detected on any specified UART communication ports even though i have the board connected and it appears on the Probing UART Ports.pastedImage_7.jpg

1 解決策
2,535件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

I assume that your board is connected through the OSBDM or BDM interface.

Please follow the steps below:

1. Go to menu Tools -> Connection Wizard -> Next 

2. Choose the "Connect through a debugger probe or on-board debugger interface" -> Next -> Next

pastedImage_2.png

3. Click on the Plug-in Configuration

4. Select " P&E OSBDM" or "P&E HCS12Z" (it depends which interface you use), after that you can Test Connection -> Ok -> Ok -> Finish

After that, it should be connected.

I hope it helps.

Best Regards,

Diana

元の投稿で解決策を見る

3 返答(返信)
2,536件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

I assume that your board is connected through the OSBDM or BDM interface.

Please follow the steps below:

1. Go to menu Tools -> Connection Wizard -> Next 

2. Choose the "Connect through a debugger probe or on-board debugger interface" -> Next -> Next

pastedImage_2.png

3. Click on the Plug-in Configuration

4. Select " P&E OSBDM" or "P&E HCS12Z" (it depends which interface you use), after that you can Test Connection -> Ok -> Ok -> Finish

After that, it should be connected.

I hope it helps.

Best Regards,

Diana

2,535件の閲覧回数
efrain_castro
Contributor II

Thanks a lot, it works with the P&E HCS12Z configuration but i seem to run into another problem, because I'm using the devkit-zvl128 connected to a TouchPAD i want to measure the touch with freemaster, the problem is that freemaster can't detect the touch even tought the program I'm using turns on a LED when i touch one of the electrodes of the PAD and the freemaster program has the electrodes variables so the measure should appear but  it doesn't. What can i do.

0 件の賞賛
返信
2,535件の閲覧回数
efrain_castro
Contributor II

Forget it i used a P&E micro multilink universal for  the measure thanks you because the configuration is the same.

0 件の賞賛
返信