How I add another ADC channel on DMA that set on example?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How I add another ADC channel on DMA that set on example?

994 次查看
kwonym
Contributor II

Hi, I use Differential ADC0 of DMA.

It used by example code.

But I don't know about how I add ADC1 channel that set on DMA.

I have been added ADC1 to code that use example.

but, result wasn't input on ADC1

About ADC0, It is on example.

About ADC1, It is my code.

//**** PDB config **********************************************************

  PDBCH0TRG0_Init (PDB_PRETRG_ON_DEALYED_CONFIG, 0x0010);

  //PDBCH0TRG1_Init (PDB_PRETRG_ON_DEALYED_CONFIG, 0x0010);

  PDB_Init (PDB_MODULE_SWTRG_NO_IRQ_CONFIG( PDB_PRESCALER_1, PDB_MULT_1, 0x1000, 0xFFFF), 1, NULL);

 

  //**** ADC config **********************************************************

  //**** ADC calibrations **************************************************

  ADC_ExecCalib (ADC0,ADC_MODULE_16B_IREF_HWTRG_CONFIG_U, &ram_adc0);       //DC OK, AC??

  //ADC_ExecCalib (ADC1,ADC_MODULE_16B_IREF_HWTRG_CONFIG_U, &ram_adc1);       //DC OK, AC??

 

  //**** ADC0,ADC1 initialization ******************************************

  ADC_Init  (ADC0, ADC_MODULE_16B_HWTRG_DMA_IREF_USER_CONFIG, ADC_CH_DI_POLL_CONFIG(DAD0), ADC_CH_DI_POLL_CONFIG(DAD0), 2, NULL);

  //ADC_Init  (ADC1, ADC_MODULE_16B_HWTRG_DMA_IREF_USER_CONFIG, ADC_CH_DI_POLL_CONFIG(DAD3), ADC_CH_DI_POLL_CONFIG(DAD3), 3, NULL);

 

  //**** DMA channel 0 *****************************************************

  DMACH0_CH1_Init();

  //DMACH1_CH1_Init();

  //**** Enable all interrupts ***********************************************

 

  EnableInterrupts;

  //**** Start PDB ***********************************************************

  PDB0_Trigger();

void DMACH0_CH1_Init(void)

  //****************************************************************************
  //**** DMA channel 0, use for Write ADC mux channel, form SRAM to ADC ********        101page datasheet
  //****************************************************************************
  DMAMUX0_CHCFG0           = DMAMUX_CHCFG_ENBL_MASK|DMAMUX_CHCFG_SOURCE(54);   //DMA source DMA Mux
  DMA_TCD0_SADDR          = (uint32) &uc_adc0_mux[0];                            //New mux setiing
  DMA_TCD0_SOFF           = 0x01;                                               //Source address increment, adding "1"
  DMA_TCD0_SLAST          = (uint32) -3;                                        //Source address decrement after major loop complete
  DMA_TCD0_DADDR          = (uint32) &ADC0_SC1A;                                //Destination address ADC0 mux selector
  DMA_TCD0_DOFF           = 0x00;                                               //Destination address increment, adding "0"
  DMA_TCD0_DLASTSGA       = 0x00;                                               //Destination address shift, go to back to [0]
  DMA_TCD0_NBYTES_MLNO    = 0x01;                                               //No of bytes minor loop
  DMA_TCD0_BITER_ELINKNO  = 0x03;                                               //Major loop step, 3 ADC channel are scaning
  DMA_TCD0_CITER_ELINKNO  = 0x03;                                               //Major loop step, 3 ADC channel are scaning
  DMA_TCD0_ATTR           = DMA_ATTR_SSIZE(0)|DMA_ATTR_DSIZE(0);                //Source a destination size, 8bit
  DMA_TCD0_CSR            = 0x0000;                                             //
 
  //****************************************************************************
  //**** DMA channel 1, use for Read ADC result data, form ADC to SRAM *********
  //****************************************************************************
  NVIC_SetIsr(INT_DMA1_DMA17,2);                                                      //17

  DMAMUX0_CHCFG1           = DMAMUX_CHCFG_ENBL_MASK|DMAMUX_CHCFG_SOURCE(40);   //DMA source ADC0
  DMA_TCD1_SADDR          = (uint32) &ADC0_RA;                                  //Source address ADC0 result register
  DMA_TCD1_SOFF           = 0x00;                                               //Source address increment, adding "0"
  DMA_TCD1_SLAST          = 0x00;                                               //Source address decrement after major loop complete
  DMA_TCD1_DADDR          = (uint32) &i_adc0_result[0];                         //Destination address, ADC0 result buffer
  DMA_TCD1_DOFF           = 0x02;                                               //Destination address increment, adding "+2"
  DMA_TCD1_DLASTSGA       = (uint32) -6;                                       //Destination address decrement after major loop complete
  DMA_TCD1_NBYTES_MLNO    = 0x02;                                               //No of bytes minor loop, 16bit ADC result
  DMA_TCD1_BITER_ELINKNO  = (DMA_BITER_ELINKNO_ELINK_MASK|0x0000|0x03);         //Channel 0 Link, Channel 0, Major loop step 3 x 4 = 12
  DMA_TCD1_CITER_ELINKNO  = (DMA_CITER_ELINKNO_ELINK_MASK|0x03);                //Channel 0 Link, Major loop step 3 x 4 = 12
  DMA_TCD1_ATTR           = DMA_ATTR_SSIZE(1)|DMA_ATTR_DSIZE(1);                //Source a destination size, 16bit
  DMA_TCD1_CSR            = (DMA_CSR_MAJORLINKCH(0)|DMA_CSR_MAJORELINK_MASK)|   //Major loop finished start request for Channel 0
                            DMA_CSR_INTMAJOR_MASK; //|DMA_CSR_INTHALF_MASK;     //Irq. enable, full transfer, half complet transfer
  DMA_ERQ                |= DMA_ERQ_ERQ1_MASK;                                  //HW request enable

}

void DMACH1_CH1_Init(void)

  //****************************************************************************
  //**** DMA channel 0, use for Write ADC mux channel, form SRAM to ADC ********        101page datasheet
  //****************************************************************************
  DMAMUX1_CHCFG0           = DMAMUX_CHCFG_ENBL_MASK|DMAMUX_CHCFG_SOURCE(55);   //DMA source DMA Mux
  DMA_TCD2_SADDR          = (uint32) &uc_adc1_mux[0];                            //New mux setiing
  DMA_TCD2_SOFF           = 0x01;                                               //Source address increment, adding "1"
  DMA_TCD2_SLAST          = (uint32) -3;                                        //Source address decrement after major loop complete
  DMA_TCD2_DADDR          = (uint32) &ADC1_SC1A;                                //Destination address ADC0 mux selector
  DMA_TCD2_DOFF           = 0x00;                                               //Destination address increment, adding "0"
  DMA_TCD2_DLASTSGA       = 0x00;                                               //Destination address shift, go to back to [0]
  DMA_TCD2_NBYTES_MLNO    = 0x01;                                               //No of bytes minor loop
  DMA_TCD2_BITER_ELINKNO  = 0x03;                                               //Major loop step, 3 ADC channel are scaning
  DMA_TCD2_CITER_ELINKNO  = 0x03;                                               //Major loop step, 3 ADC channel are scaning
  DMA_TCD2_ATTR           = DMA_ATTR_SSIZE(0)|DMA_ATTR_DSIZE(0);                //Source a destination size, 8bit
  DMA_TCD2_CSR            = 0x0000;                                             //
 
  //****************************************************************************
  //**** DMA channel 1, use for Read ADC result data, form ADC to SRAM *********
  //****************************************************************************
  NVIC_SetIsr(INT_DMA3_DMA19,3);                                                      //17

  DMAMUX1_CHCFG1           = DMAMUX_CHCFG_ENBL_MASK|DMAMUX_CHCFG_SOURCE(41);   //DMA source ADC1
  DMA_TCD3_SADDR          = (uint32) &ADC1_RA;                                  //Source address ADC0 result register
  DMA_TCD3_SOFF           = 0x00;                                               //Source address increment, adding "0"
  DMA_TCD3_SLAST          = 0x00;                                               //Source address decrement after major loop complete
  DMA_TCD3_DADDR          = (uint32) &i_adc1_result[0];                         //Destination address, ADC0 result buffer
  DMA_TCD3_DOFF           = 0x02;                                               //Destination address increment, adding "+2"
  DMA_TCD3_DLASTSGA       = (uint32) -6;                                       //Destination address decrement after major loop complete
  DMA_TCD3_NBYTES_MLNO    = 0x02;                                               //No of bytes minor loop, 16bit ADC result
  DMA_TCD3_BITER_ELINKNO  = (DMA_BITER_ELINKNO_ELINK_MASK|0x0000|0x03);         //Channel 0 Link, Channel 0, Major loop step 3 x 4 = 12
  DMA_TCD3_CITER_ELINKNO  = (DMA_CITER_ELINKNO_ELINK_MASK|0x03);                //Channel 0 Link, Major loop step 3 x 4 = 12
  DMA_TCD3_ATTR           = DMA_ATTR_SSIZE(1)|DMA_ATTR_DSIZE(1);                //Source a destination size, 16bit
  DMA_TCD3_CSR            = (DMA_CSR_MAJORLINKCH(0)|DMA_CSR_MAJORELINK_MASK)|   //Major loop finished start request for Channel 0
                            DMA_CSR_INTMAJOR_MASK; //|DMA_CSR_INTHALF_MASK;     //Irq. enable, full transfer, half complet transfer
  DMA_ERQ                |= DMA_ERQ_ERQ3_MASK;                                  //HW request enable

}

0 项奖励
回复
1 回复

717 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Kwon,

In term of the codes you provided above, I found that the example code and yours both use the DMA Channel0 and Channel1.

I've like to suggest that you should choose other channels for the ADC1 except the Channel0 and Channel1.

Hope my reply helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复