High Speed RNDIS and CDC composite (?)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

High Speed RNDIS and CDC composite (?)

1,213 Views
mjbcswitzerland
Specialist V

Hi All

I am wondering whether anyone has used RNDIS + CDC composite on a K61 or K70's HS USB interface?

The issue that I have is that I can do this on any FS USB interface since they have 16 endpoints but the K61/K70's HS USB has just 4 and this configuration essentilly needs 5:

- Endpoint 0 - control

- Endpoint 1 - RNDIS bulk IN/OUT

- Endpoint 2 - RNDIS interrupt

- Endpoint 3 - CDC bulk IN/OUT

- Endpoint 4 - CDC interrupt

In fact the CDC interrupt endpoint is not used in practice but I don't know whether there is any way to configure so that it is not needed to satisfy the host or whether there is some other trick to get around this.

Any ideas (without having to move to K66 with 8 HS endpoints)???

Regards

Mark

Labels (1)
0 Kudos
Reply
0 Replies