Hi

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hi

2,030件の閲覧回数
kirankumars
Contributor I

1)i am using TRK-KEA128 board can you tell how to configure bus clock for 16M. I am using internal oscillator right no it is 20M.

2)How to calculate the CAN baud rate for 125K with bus clock of 20M and also for 16M..?

0 件の賞賛
返信
2 返答(返信)

1,948件の閲覧回数
egoodii
Senior Contributor III

It is not possible to get any derivation from the internal clock to be accurate enough to enable proper CAN bit tolerance.

0 件の賞賛
返信

1,948件の閲覧回数
david_diaz
NXP Employee
NXP Employee

Hello,

I am afraid that 20 MHz is the closest bus frequency value you can get using the internal oscillator.

In case you need to get 16 MHz bus frequency, I recommend using an external oscillator.

The KEA128 supports 32.768 kHz crystal or 4 MHz to 24 MHz crystal or ceramic resonator.

Regarding the CAN bit rate, please refer to the Clock system at chapter 32.4.5.2 from the Reference Manual at the following link:

http://www.freescale.com/files/microcontrollers/doc/ref_manual/KEA128RM.pdf

Hope this information will be useful for you.

Have a great day.

David

0 件の賞賛
返信