Hi,everyone! I am using the KL17 microcontroller in recent days. Now I meet a problem. The question is:can the KL17 work without external oscillator? In other words,if the EXTAL0 and XTAL0 pins are floating that connect to nothing,will the KL17 work norma

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi,everyone! I am using the KL17 microcontroller in recent days. Now I meet a problem. The question is:can the KL17 work without external oscillator? In other words,if the EXTAL0 and XTAL0 pins are floating that connect to nothing,will the KL17 work norma

1,363 Views
haoyuluo
Contributor I

     Hi,everyone!

     I am using the KL17 microcontroller in recent days. Now I meet a problem. The question is:can the KL17 work without external oscillator? In other words,if the EXTAL0 and XTAL0 pins are floating that connect to nothing,will the KL17 work normally? If the KL17 can,how should I set up the KL17 in the program? I have set MCG to HIRC mode or LIRC2M mode,but the KL17 didn’t work.

     I need your help urgently. Who can help me?

Labels (1)
0 Kudos
Reply
2 Replies

1,197 Views
mjbcswitzerland
Specialist V

Hi

Download the open source uTasker project from GIT hub (link below).
Select KL27 (eg. FRDM_KL27Z) in config.h (without enabling USB, so that it also works on KL17) and set the define RUN_FROM_HIRC in app_hw_kinetis.h.
This will give you an operating project on any KL27 / KL17 board.
Finally check the clock code in _LowLevelInit() that is being selected by the configuration - copy it to solve problems in whatever environment you use.

Regards

Mark

Kinetis: http://www.utasker.com/kinetis.html
Kinetis KL25, KL26, KL27, KL28, KL82:
- http://http://www.utasker.com/kinetis/FRDM-KL25Z.html
- http://www.utasker.com/kinetis/TWR-KL25Z48M.html
- http://www.utasker.com/kinetis/FRDM-KL26Z.html
- http://www.utasker.com/kinetis/TEENSY_LC.html
- http://www.utasker.com/kinetis/FRDM-KL27Z.html
- http://www.utasker.com/kinetis/Capuccino-KL27.html
- http://www.utasker.com/kinetis/FRDM-KL28Z.html
- http://www.utasker.com/kinetis/FRDM-KL82Z.html

Build with: CW10.x, KDS, MCUXpresso, IAR, Keil, Greenhills, Crossworks, CooCox, Atollic, S32 Design Studio, GNU Make and Visual Studio

Free Open Source solution: https://github.com/uTasker/uTasker-Kinetis
Working project in 15 minutes video: https://youtu.be/K8ScSgpgQ6M

For better, faster, cheaper product developments consider the uTasker developer's version, professional Kinetis support, one-on-one training and complete fast-track project solutions to set you apart from the herd : http://www.utasker.com/support.html

0 Kudos
Reply

1,197 Views
miguel_mendoza
NXP Employee
NXP Employee

Hi Haoyu Luo,

The question is: can the KL17 work without external oscillator?
Yes, It can. Actually, all kinetis devices work in default mode without an external oscillator.

how should I set up the KL17 in the program?

I recommend Clock config tools that come along with the use of SDK  you can download it in the web page: Welcome | MCUXpresso SDK Builder , inside this page there is an online Clock config tool, so you can generate the files and copy them into your project.

regards,
Miguel

0 Kudos
Reply