Hi There, I wanted to know if I could use the CMSIS header files from the kinectis SDK or sample code to add KINECTIS support to other projects such as RIOT, CHIBIOS, opencm3?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi There, I wanted to know if I could use the CMSIS header files from the kinectis SDK or sample code to add KINECTIS support to other projects such as RIOT, CHIBIOS, opencm3?

792 Views
raghavaaditya
Contributor I

-

Labels (1)
0 Kudos
Reply
1 Reply

726 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Raghava,

Although I do not know the CHIBIOS OS and the RIOT game, I think it is okay to use CMSIS header from the Kinetis SDK, because we provide the source code of CMSIS and header file, you can add the source code file to your system.

Hope it can help you.

BR

XiangJun Rong

0 Kudos
Reply