Help with KwikStik j-link flashing external device.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help with KwikStik j-link flashing external device.

Jump to solution
2,597 Views
luisf_rossi
Contributor II

Hi, i am trying to use the KwikStik j-link to flash an external Kinetis. For some reason it is not working and CodeWarrior is retrieving a message saying it could not reset the Kinetis.

 

I even tryed to remove the kinetis on the KwikStik board but with no change.

 

The Kinetis connections can be seen on the atachement. Thats just a piece of the board but related to kinetis there are just some extra decoupling network on other sheets.

 

The cable and pinheaders i am using are the sugested by the manual.

the j-link connector is pretty close to the kinetis..

 

 

Any help is appreciated.

0 Kudos
Reply
1 Solution
2,062 Views
luisf_rossi
Contributor II

Ok got the problem.. athought the kwikstick is the Version 4 it still can't program external devices with the switch off.. turning on worked here...

 

Thank you

View solution in original post

0 Kudos
Reply
1 Reply
2,063 Views
luisf_rossi
Contributor II

Ok got the problem.. athought the kwikstick is the Version 4 it still can't program external devices with the switch off.. turning on worked here...

 

Thank you

0 Kudos
Reply