Help selecting Kinetis MCU for inhouse project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help selecting Kinetis MCU for inhouse project

628 Views
niklascooke
Contributor I

Hi,

Im looking for a Kinetis MCU which has this specification:

>= 120MHz
>= 128kB RAM
>= 256kB FLASH
> 4 ch 16bit SE ADCs
2xUSB OTG
2xCAN

I have come up with theese MCUs but im not sure if all of the SE ADCs are 16bit resolution ?

MK24FN1M0VDC12R
* MK60FN1M0VMD15
MK64FN1M0VDC12
MK82FN256VDC15

MK60 is our primary choice at the moment, but still unsure about the ADC resolution.


Best regards Niklas Cooke
HW Engineer

0 Kudos
Reply
1 Reply

559 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Niklas,

The best choice based on your requirements is the MK60FN1M0VMD15 part. Regarding the ADC, it does have the 16-bit resolution you require.

Hope it helps!

Best Regards,

Carlos Mendoza

Technical Support Engineer

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply