Help control TWRPI-SLCD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help control TWRPI-SLCD

3,535件の閲覧回数
phamminhthuan
Contributor II

Hello every body. I'm trying to control TWRPI-SLCD module on TWR-K53N512 kit. But I'm beginer in ARM microctroller so that I can't understand how  to control it.

Do you have any library or example control it with IAR Embedded Workbend for ARM? I also need help about I2C communication with Kit.

I hope to rececive helps from all of you. Thanks you very much!

タグ(2)
0 件の賞賛
返信
5 返答(返信)

3,229件の閲覧回数
EarlOrlando
Senior Contributor II

Hello Pham Minh Thuan,

Are you working with or without KSDK? The SLCD peripheral is supported in KSDK which will make easier the implementation.

Also you can take a look into this SLCD document​ from Mark Butcher to see how it works and this application note (AN3412)​ which uses this module. I recommend to read the chapter 58 SLCD from the K53 Reference Manual​.

I attached some files used for the FRDM-KL46Z to use its display with the SLCD module for reference. In this example you must initialize the module calling vfnLCD_Init() and you can change the display message calling vfnLCD_Write_Msg(uint8_t *lbpMessage).

Hope this helps.

Best regards,

Earl.

0 件の賞賛
返信

3,229件の閲覧回数
phamminhthuan
Contributor II

Thank you very much!

I'm beginer in ARM and I'm using TWR-K53N512 Kit to run demo MED-SPO2 in my final Project at University. Now, I want to control SLCD module include in TWR-K53N512 module to display value of Heart Rate or SpO2. I also want to control I2C to display on another LCD. But I don't use KSDK. I'm using IAR because MED-SPO2 was developed on IAR.

I read many documents of freescale but I can't understand it. I think because I'm beginer in ARM MCU so that I can't understand all of them.

I'm Vietnamese and my English is not good. I think I have many mistake in spelling and Grammar when Writing in this discussion.

Can you help me about IAR?

Thanks!

0 件の賞賛
返信

3,229件の閲覧回数
EarlOrlando
Senior Contributor II

Hello again,

If you need help to get started with IAR I recommend you to read this user guide. In the chapter two there are a series of tutorials to learn to use the tool.

Best regards,

Earl.

0 件の賞賛
返信

3,229件の閲覧回数
phamminhthuan
Contributor II

Thank you very much.

Do you have libraries of K53N512 MCU for IAR? I searched on Freescale, but I did'nt find them. STM32 or STM8 of ST. ST supported library for IAR, but Freescale I can't find on website. Can you give them to me?

Thank you.

0 件の賞賛
返信

3,229件の閲覧回数
mjbcswitzerland
Specialist V

Hi

You can get TWR-K53N512 support, including full IAR compatibility, at µTasker Kinetis TWR-K53N512 support

Attached is an executable that also shows the SLCD operating on this board. It needs no installation - just unzip and execute the uTasker.exe.

Regards

Mark

Kinetis: µTasker Kinetis support

K53: µTasker Kinetis TWR-K53N512 support

SLCD: http://www.utasker.com/docs/uTasker/uTasker_SLCD.pdf

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 件の賞賛
返信