Help clearing SPI TX buffers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help clearing SPI TX buffers

4,132件の閲覧回数
markosiponen
Contributor III

I'm using a MK10FN1M0VLQ12.


I have setup DMA to transfer data to SPI2_PUSHR.


I have not enabled TX FIFO or RX FIFO for the SPI.


I see that when I enable the DMA channel the DMA immediatly transfers 2 byte. Why is this happening. Why not only one byte? Is the SPI2_PUSHR double buffered?


And another problem. When SPI chip select goes high I need to reset the DMA and also any possible outgoing data in the SPI. How can I reset the SPI TX buffers?

What I mean is if SR[TFFF] is 0 (TX FIFO is full) how do i get it to become 1 (TX FIFO is not full)?



Update:


Now I have tested an approach here. I have found that the following works:


    // Disable DMA MUX 0 channel first before we change anything

    DMAMUX0->CHCFG[MAIN_SPI_TX_DMA_CH] = 0;

    DMA0->CERQ = MAIN_SPI_TX_DMA_CH; // Disable DMA Request

  

    // Halt SPI

   SPI2->MCR |=  SPI_MCR_HALT_MASK;

  

    //Clear TX FIFO

    SPI2->MCR |= SPI_MCR_CLR_TXF_MASK;

  

    // Unhalt SPI

    SPI2->MCR &= (uint32_t)~(uint32_t)(SPI_MCR_HALT_MASK);

    Setup the DMA

    ...

    // Enables DMA channel and select DMA MUX Request Sources for the DMA Channel

    DMAMUX0->CHCFG[MAIN_SPI_TX_DMA_CH] = DMAMUX_CHCFG_SOURCE(21) | DMAMUX_CHCFG_ENBL_MASK; // 21 = SPI2 Transmit


I must halt the SPI2 and then clear the TX FIFO. Else it will not work.


Is this the correct way to do it?



0 件の賞賛
返信
1 返信

2,041件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I do a test with K60_100MHz DSPI module and check when write a byte to SPI_PUSHR register how many bytes the SPI will transfer. The result is only one.

Please refer below code to disable TX/RX FIFO and Clear TX/RX counter during SPI initialization.

spi.png

And it need to set SPIx_CTARn register [FMSZ] bits value to 0x7 for a byte data transfer.

The test software source code is based on spi_demo from below link:

KINETIS512_V2_SC  (Kinetis 100MHz Rev 2 Example Projects):

Kinetis K60 100 MHz MCU Tower System Module|Freescale


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信