Help! Warning "failed to initialize pemicro interface dll"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help! Warning "failed to initialize pemicro interface dll"

3,368件の閲覧回数
w_x
Contributor II

While using TWR board, I tryed to download code to target in IAR, It showed this message  "failed to initialize pemicro interface dll". What's the problem? Anyone can help?

0 件の賞賛
返信
2 返答(返信)

2,787件の閲覧回数
J2MEJediMaster
Specialist I

You are missing the driver for your run controller/emulator probe. If you are using a P&E Microsystems probe or a Freescale TAP (which amounts to the same thing), you can download the drivers at www.pemicro.com.

 

---Tom

0 件の賞賛
返信

2,787件の閲覧回数
ahmedrida
Contributor III

Hello, I'm having the same problem using TWR vf65gs10 board, trying to run an example for my board but cant' connect to target. I get the same message or the message :

Target is running. Stop target ? I reset the target put yes and the same message comes.

Anyone can help ?

0 件の賞賛
返信