Hello world program for Kinetis

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Hello world program for Kinetis

跳至解决方案
7,497 次查看
FabianS
Contributor II

Hello,

 

I am trying to write a small hello world program for the Kinetis K60 but it's not working. It's just a pin I want to toggle.

[code]

#include <stdio.h>

#include "derivative.h" /* include peripheral declarations */

int main()
{
    //MCU_init();
    
    GPIOC_POER |= (1<<0);
    while(1)
    {
        printf("Hello World!\n");
        GPIOC_PTOR = (1<<0);
    }
    return 0;
}
[/code]

Using MCU_init or not makes no difference. The pin simply does nothing.

I also tryed to use a DAC but when I add the DAC0 settings in the "Target CPU" view the program crashes and jumps to PE_ISR(isrINT_NMI) when calling the MCU_init method.

 

PS: Why is here no extra forum for Kinetis?

0 项奖励
回复
1 解答
5,063 次查看
MikeRC
Contributor III

Try this for the main function:

 

int main()
{
    //MCU_init();
    

    SIM_SCGC5 = 0x800;

    PORTC_PCR0 = 0x00000100;


    GPIOC_POER |= (1<<0);
    while(1)
    {
        printf("Hello World!\n");
        GPIOC_PTOR = (1<<0);
    }
    return 0;
}

 

The GPIO is a lot different for Kinetis than it used to be for Star 12's.  The PortC clock needs to be enabled and the Pin Mux needs to be set to use the GPIO functionality.

-Mike

在原帖中查看解决方案

0 项奖励
回复
2 回复数
5,064 次查看
MikeRC
Contributor III

Try this for the main function:

 

int main()
{
    //MCU_init();
    

    SIM_SCGC5 = 0x800;

    PORTC_PCR0 = 0x00000100;


    GPIOC_POER |= (1<<0);
    while(1)
    {
        printf("Hello World!\n");
        GPIOC_PTOR = (1<<0);
    }
    return 0;
}

 

The GPIO is a lot different for Kinetis than it used to be for Star 12's.  The PortC clock needs to be enabled and the Pin Mux needs to be set to use the GPIO functionality.

-Mike

0 项奖励
回复
5,063 次查看
anthony_huereca
NXP Employee
NXP Employee

You can also look at the GPIO example in the Kinetis Sample Code for more examples of blinking the LED's: http://www.freescale.com/webapp/sps/download/license.jsp?colCode=KINETIS512_SC