I am working on a custom board that has MK60DN512ZVLQ10 uC on it...
Tower board has Ethernet in RM-II interface mode...
Our team mates have interfaced Ethernet in M-II mode which needs PTA-(24-29) to be set in ALT-4 MUX functionality.
I got it working with FNET's TCP stack with the above changes but we really need it work as well as with RTCS stack.
Tools: CW10.2/ Keil & MQX4.0.1 ---- Debugger: PE micro universal Multilink.
regards ...........
已解决! 转到解答。
Hi
I believe that you need to add additional lines as follows (as well as A24..A29):
| _CONFIG_PERIPHERAL(A, 9, PA_9_MII0_RXD3); | // MII0_RXD3 on PA.9 (alt. function 4) | |
| _CONFIG_PERIPHERAL(A, 10, PA_10_MII0_RXD1); | // MII0_RXD1 on PA.10 (alt. function 4) | |
| _CONFIG_PERIPHERAL(A, 11, PA_11_MII0_RXCLK); | // MII0_RXCLK on PA.11 (alt. function 4) | |
| _CONFIG_PERIPHERAL(A, 24, PA_24_MII0_TXD2); | // MII0_TXD2 on PA.24 (alt. function 4) | |
| _CONFIG_PERIPHERAL(A, 25, PA_25_MII0_TXCLK); | // MII0_TXCLK on PA.25 (alt. function 4) | |
| _CONFIG_PERIPHERAL(A, 26, PA_26_MII0_TXD3); | // MII0_TXD3 on PA.26 (alt. function 4) | |
| _CONFIG_PERIPHERAL(A, 27, PA_27_MII0_CRS); | // MII0_CRS on PA.27 (alt. function 4) | |
| _CONFIG_PERIPHERAL(A, 28, PA_28_MII0_TXER); | // MII0_TXER on PA.28 (alt. function 4) | |
| _CONFIG_PERIPHERAL(A, 29, PA_29_MII0_COL); | // MII0_COL on PA.29 (alt. function 4) |
I use the following macro for peripheral functions:
#define _CONFIG_PERIPHERAL(port, pin, function) SIM_SCGC5 |= SIM_SCGC5_PORT##port; PORT##port##_PCR##pin = function
where each alternative function 4 is simply 0x00000400 (eg. PA_9_MII0_RXD3 is defined as this).
Regards
Mark
Hi
I believe that you need to add additional lines as follows (as well as A24..A29):
| _CONFIG_PERIPHERAL(A, 9, PA_9_MII0_RXD3); | // MII0_RXD3 on PA.9 (alt. function 4) | |
| _CONFIG_PERIPHERAL(A, 10, PA_10_MII0_RXD1); | // MII0_RXD1 on PA.10 (alt. function 4) | |
| _CONFIG_PERIPHERAL(A, 11, PA_11_MII0_RXCLK); | // MII0_RXCLK on PA.11 (alt. function 4) | |
| _CONFIG_PERIPHERAL(A, 24, PA_24_MII0_TXD2); | // MII0_TXD2 on PA.24 (alt. function 4) | |
| _CONFIG_PERIPHERAL(A, 25, PA_25_MII0_TXCLK); | // MII0_TXCLK on PA.25 (alt. function 4) | |
| _CONFIG_PERIPHERAL(A, 26, PA_26_MII0_TXD3); | // MII0_TXD3 on PA.26 (alt. function 4) | |
| _CONFIG_PERIPHERAL(A, 27, PA_27_MII0_CRS); | // MII0_CRS on PA.27 (alt. function 4) | |
| _CONFIG_PERIPHERAL(A, 28, PA_28_MII0_TXER); | // MII0_TXER on PA.28 (alt. function 4) | |
| _CONFIG_PERIPHERAL(A, 29, PA_29_MII0_COL); | // MII0_COL on PA.29 (alt. function 4) |
I use the following macro for peripheral functions:
#define _CONFIG_PERIPHERAL(port, pin, function) SIM_SCGC5 |= SIM_SCGC5_PORT##port; PORT##port##_PCR##pin = function
where each alternative function 4 is simply 0x00000400 (eg. PA_9_MII0_RXD3 is defined as this).
Regards
Mark
Thank you Mark
I added the following lines in the function "_bsp_enet_io_init" found in "init_gpio.c" file and Ethernet started to work fine....
| pctl->PCR[5] = 0x00000400; | /* PTA5, RMII0_RXER/MII0_RXER | */ |
| pctl->PCR[9] = 0x00000400; | /* PTA9, MII0_RXD3 | */ |
| pctl->PCR[10] = 0x00000400; | /* PTA10, MII0_RXD2 | */ |
| pctl->PCR[11] = 0x00000400; | /* PTA11, MII0_RXCLK | */ |
| pctl->PCR[24] = 0x00000400; | /* PTA24, MII0_TXD2 | */ |
| pctl->PCR[25] = 0x00000400; | /* PTA25, MII0_TXCLK | */ |
| pctl->PCR[26] = 0x00000400; | /* PTA26, MII0_TXD3 | */ |
| pctl->PCR[27] = 0x00000400; | /* PTA27, MII0_CRS | */ |
| pctl->PCR[28] = 0x00000400; | /* PTA28, MII0_TXER | */ |
| pctl->PCR[29] = 0x00000400; | /* PTA29, MII0_COL | */ |
Regards