Header file for KL17

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Header file for KL17

1,602 Views
marlonsmith
Contributor IV

Hi everyone,

I'm starting a new project using an MKL17Z32 part.  For the other Kinetis parts I've used, I've been able to use processor expert to generate driver code.  I've also been able to find header files for use with the processor.

For example, with a K20 chip I was able to go here: K20_100 |Kinetis 20 100 MHz MCUs|NXP and under the section "Snippets, Boot Code, Headers, Monitors, etc." I can download headers for use with the chip.

For the K1x parts, there aren't any headers listed there.

Does anyone know where I can find the headers?  Or is there an update to Processor Expert that supports this part?

Thanks!

Marlon

Tags (1)
0 Kudos
Reply
1 Reply

1,470 Views
miduo
NXP Employee
NXP Employee

Hi,

Please make this post as reference for this issue:KL17 example

0 Kudos
Reply