Header file for KL17

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Header file for KL17

1,624件の閲覧回数
marlonsmith
Contributor IV

Hi everyone,

I'm starting a new project using an MKL17Z32 part.  For the other Kinetis parts I've used, I've been able to use processor expert to generate driver code.  I've also been able to find header files for use with the processor.

For example, with a K20 chip I was able to go here: K20_100 |Kinetis 20 100 MHz MCUs|NXP and under the section "Snippets, Boot Code, Headers, Monitors, etc." I can download headers for use with the chip.

For the K1x parts, there aren't any headers listed there.

Does anyone know where I can find the headers?  Or is there an update to Processor Expert that supports this part?

Thanks!

Marlon

タグ(1)
0 件の賞賛
返信
1 返信

1,492件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Please make this post as reference for this issue:KL17 example

0 件の賞賛
返信