Have you any reference code for RAM test of external DDR2 on the K70 kinetis

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Have you any reference code for RAM test of external DDR2 on the K70 kinetis

1,191 次查看
poul-erikhansen
Contributor II

I am worried that any error must be hidden by a catch function.


Poul-Erik.



标签 (1)
0 项奖励
回复
1 回复

912 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please refer attached SRAM memory test code for internal SRAM, which is also suitable with DDR2 memory test.

About K70 DDR2 memory controller setting, please download KINETIS_K70_DDR_INIT (Kinetis K70 DDR memory initialization tool) from below link:

K70_120: Kinetis K70 Graphic LCD 120/150 MHz MCUs
Wish it help.

best regards,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------