Has anyone coded up a bit banged SPI driver for a L series device?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Has anyone coded up a bit banged SPI driver for a L series device?

2,252 Views
clivepalmer
Contributor III

Hi

I am using a KL02Z device which only has a single SPI port. I require to use two and hence I need to code up a bit bashed SPI driver.

Before I spend time coding and debugging this, is there anyone out there who has already coded one up that they would be so kind as to share?

Thanks

3 Replies

1,496 Views
perlam_i_au
Senior Contributor I

There is not an specific driver for KL02Z, but you can use as base the SPI driver for KL05 (attached).


Have a nice day,
Perla Moncada

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,496 Views
mjbcswitzerland
Specialist V

Clive

I use this code to bit bang to EZPORT of other devices. There is no difference between K and KL GPIO port code.

- The ports need first to be configured as inputs or outputs before use.

- the clock phase matches the EZPORT so may need to be adjusted for certain SPI slaves

- port used and ports bits may need to be changed to suit

- whether setup and hold delays are required depends on your CPU speed and the SPI slave's speed. I needed 1us delays for the EZPORT to work when using the code on 100MHz devices because the GPIOx_PSOR and GPIOx_PCOR operations are pretty fast.

#define EZRESETOUT      PORTD_BIT15                              // port output for reset signal
#define EZCSOUT        PORTD_BIT11                              // SPI2_SC0
#define EZDIN          PORTD_BIT13                              // SPI2_MOSI
#define EZDOUT          PORTD_BIT13                              // SPI2_MISO
#define EZCLKOUT        PORTD_BIT12                              // SPI2_CLK

// Send and receive a single byte

//

static unsigned char fnSendEZPORT(unsigned char ucDataOut)

{

unsigned char ucBit = 0x80;                                      // data sent and receive most significant bit first
unsigned char ucReadByte = 0;
do {
   GPIOD_PSOR = EZCLKOUT;                                      // generate rising clock edge
   fnDelayLoop(1);
   if (ucDataOut & ucBit) {                                    // set new data output state
       GPIOD_PSOR = EZDOUT;
   }
   else {
       GPIOD_PCOR = EZDOUT;
   }
   fnDelayLoop(1);
   GPIOD_PCOR =  = EZCLKOUT;                                    // falling clock edge
   fnDelayLoop(1);             
   GPIOD_PSOR = EZCLKOUT;                                      // rising clock edge
   if (GPIOD_PDIR & EZDIN) {                                    // read data in
       ucReadByte |= ucBit;
   }
   ucBit >>= 1;
} while (ucBit != 0);
return ucReadByte;

}


Regards

Mark


1,496 Views
clivepalmer
Contributor III

Hi,

Thanks you both for taking the time to reply and sorry for my late response. This help is much appreciated.

0 Kudos
Reply