Hardwarerequirements for the MKL26Z128VLH4 SWD-Port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hardwarerequirements for the MKL26Z128VLH4 SWD-Port

Jump to solution
1,718 Views
st165450
Contributor I
Hello,
im trying to design a pcb, based on a MKL26Z128VLH4.
But i'm not sure, if there are special requirements to implement the swd port. The documentation is not very helpful at this point. My question is, if it's necessary to use a special wiring for the SWD CLK- and DIO signal.
Thanks
Falk
Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,633 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Falk D .

   About the KL series hardware design, you can refer to this document:

https://www.nxp.com/webapp/Download?colCode=KLQRUG 

Chapter 2 General System Setup (Hardware Considerations)

  To the SWD interface, you need to add 10K pullup in the SWD_DIO pin.

  SWD interface need 5 pins: SWD_DIO, SWD_CLK, RESET, VDD, GND.

  Reset pin in the MCU side should add the 4.7K to 10K pull up resistor, and 0.1uf capacitor to ground.

  About the hardware wire, it is not special, just normally wire in the PCB is OK.

Wish it helps you!

If you still have questions about it, please kindly let me know.

Have a great day,

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

1 Reply
1,634 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Falk D .

   About the KL series hardware design, you can refer to this document:

https://www.nxp.com/webapp/Download?colCode=KLQRUG 

Chapter 2 General System Setup (Hardware Considerations)

  To the SWD interface, you need to add 10K pullup in the SWD_DIO pin.

  SWD interface need 5 pins: SWD_DIO, SWD_CLK, RESET, VDD, GND.

  Reset pin in the MCU side should add the 4.7K to 10K pull up resistor, and 0.1uf capacitor to ground.

  About the hardware wire, it is not special, just normally wire in the PCB is OK.

Wish it helps you!

If you still have questions about it, please kindly let me know.

Have a great day,

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------