Hardware fault when reading a register

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hardware fault when reading a register

2,195件の閲覧回数
gmgjeg
Contributor II

Hardware fault when reading a register

ラベル(1)
3 返答(返信)

2,067件の閲覧回数
mjbcswitzerland
Specialist V

Hi

Usually because the module being accessed doesn't have its clock enabled to it.
See SIM_SCGCx control.

Regards

Mark

2,067件の閲覧回数
gmgjeg
Contributor II

Thank you for the help.

On Friday, December 21, 2018, 5:56:05 AM EST, kerryzhou <[email protected]> wrote:

|

NXP Community

|

Hardware fault when reading a register

Kerry Zhou marked Mark Butcher's reply on Hardware fault when reading a register as helpful. View the full reply

Marked as helpful:

Hi

 

Usually because the module being accessed doesn't have its clock enabled to it.

See SIM_SCGCx control.

 

Regards

 

Mark

Following Hardware fault when reading a register in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

Virus-free. www.avast.com

0 件の賞賛
返信

2,067件の閲覧回数
gmgjeg
Contributor II

Thank you, I will make sure it is enabled.

On Thursday, December 20, 2018, 11:54:36 AM EST, mjbcswitzerland <[email protected]> wrote:

|

NXP Community

|

Re: Hardware fault when reading a register

reply from Mark Butcher in Kinetis Microcontrollers - View the full discussion

Hi

 

Usually because the module being accessed doesn't have its clock enabled to it.

See SIM_SCGCx control.

 

Regards

 

Mark

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in Kinetis Microcontrollers by email or at NXP Community

Following Re: Hardware fault when reading a register in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

Virus-free. www.avast.com

0 件の賞賛
返信