Hard fault caused by Processor Expert

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Hard fault caused by Processor Expert

跳至解决方案
2,788 次查看
mikethomas
Contributor II

Hello all,

 

I am a new user of the Kinetis MCU's.

I am experimenting with the Freedom board.

 

I have created a simple program on the Freedom board which blinks the RGB leds. Initially, I created the project using "Device Initialization".

Using the Hardware Prespective, I setup the LED ports and the System Timer (SysTick). I then accidentally, clicked on the "DAC0" block in the IC outline, which immediatly generated the following code in the MCUInit module...

 

 

/* ### Init_DAC init code */ 

/* DAC0_C0: DACEN=0,DACRFS=0,DACTRGSEL=0,DACSWTRG=0,LPEN=0,DACBTIEN=0,DACBBIEN=0 */ 

DAC0_C0 &= ( uint8_t)~(uint8_t)0xFBU;

 

/* DAC0_SR: DACBFRPTF=0,DACBFRPBF=0 */

 

DAC0_SR &= (uint8_t)~(uint8_t)0xFBU;

 

/* DAC0_DAT0L: DATA0=0 */

 

DAC0_DAT0L = (uint8_t)0x00U;

 

/* DAC0_DAT0H: DATA1=0 */

DAC0_DAT0H = (uint8_t)0x00U;

 

/* DAC0_C1: DMAEN=0,DACBFMD=0,DACBFEN=0 */

 

DAC0_C1 &= (uint8_t)~(uint8_t)0xE5U;

 

/* DAC0_C0: DACEN=0,DACRFS=0,DACTRGSEL=0,DACSWTRG=0,LPEN=0,DACBTIEN=0,DACBBIEN=0 */

 

DAC0_C0 &= (uint8_t)~(uint8_t)0xFBU;

 

/* ### Init_DAC init code */ 

/* CMP0_DACCR: DACEN=0,VRSEL=0,VOSEL=0 */

 

CMP0_DACCR = (uint8_t)0x00U;

 

The component inspector for the DAC shows that; pins, interrupts, and device initialization are disabled, however, code is ALWAYS generated when the  "Generate Code" button is clicked in the Hardware Prespective.

 

This in itself would not be a problem, except that apparently, a Hard Fault is generated when the first line of the DAC initialization code is executed.

     DAC0_C0 &= ( uint8_t)~(uint8_t)0xFBU;

 

According to the data sheet, this statement should do nothing more than leave the register as it was before it was called.

Commenting out the initialization code corrects the problem, and allows my test program to run fine.

 

The question is: what is this statement doing to cause a Hard Fault.

 

I have attached the entire MCUInit module which is causing the fault

 

Thanks in advance,

Mike

 

 

 

 

 

 

Original Attachment has been moved to: MCUinit.c.zip

标签 (1)
0 项奖励
回复
1 解答
2,060 次查看
JimDon
Senior Contributor III

It's because the clocks are not gated to that module, because there is no init code.

This will cause a hard fault, when you try to interact with it.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,061 次查看
JimDon
Senior Contributor III

It's because the clocks are not gated to that module, because there is no init code.

This will cause a hard fault, when you try to interact with it.

0 项奖励
回复
2,059 次查看
mikethomas
Contributor II

Thank you Jim for pointing me in the right direction.

Sure enough, when you mouse hover over the DAC clock gate settings in the Component Inspector you get a warning message.

See attached.

KLQRUG mentions the need to enable  clock gate for; DMA, ADC, UART, TPM, but I did not see it for DAC. I should've assumed.

Thanks again.

Mike

0 项奖励
回复