Hi all,
I'm having some trouble with using floating point operations on a K10. I'm compiling with gcc with -mcpu=cortex-m4 -mabi=aapcs -mthumb -msoft-float.
I get a Hard Fault exception on executing the blx instruction highlighted below:
74 subfactor = LOOP_CYCLES*1e6/cpu_clockRate;
000008c2: movw r3, #61448 ; 0xf008
000008c6: movt r3, #8191 ; 0x1fff
000008ca: ldrh r3, [r3, #0]
000008cc: mov r0, r3
000008ce: blx 0x1458 <__floatsidf> <-- Core Hard Faults here
000008d2: mov r2, r0
000008d4: mov r3, r1
000008d6: add r1, pc, #56 ; (adr r1, 0x910 <cpu_Delay+88>)
000008d8: ldrd r0, r1, [r1]
000008dc: blx 0x17c4 <__divdf3>
000008e0: mov r2, r0
000008e2: mov r3, r1
000008e4: mov r0, r2
000008e6: mov r1, r3
000008e8: blx 0x19d0 <__fixdfsi>
000008ec: mov r3, r0
000008ee: strh r3, [r7, #14]
Looking at the code for the __floatsidf, it doesn't look like thumb code? Is this right? Am I missing a compiler flag?
__floatsidf:
00001458: teq r0, #0
0000145c: moveq r1, #0
00001460: bxeq lr
00001464: push {r4, r5, lr}
00001468: mov r4, #1024 ; 0x400
0000146c: add r4, r4, #50 ; 0x32
00001470: ands r5, r0, #-2147483648 ; 0x80000000
00001474: rsbmi r0, r0, #0
00001478: mov r1, #0
0000147c: b 0x1274 <__aeabi_dadd+336>
Hi
Can you please explain where you added the -mcpu=cortex-m4 for the linker? I'm trying to add this option to the linker flags (Xlinker [option]) but it gives error.
Thanks,