HRPWM example for MKV46?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HRPWM example for MKV46?

ソリューションへジャンプ
2,199件の閲覧回数
arimendes
Contributor III

Hi,

I need an example of how to use the HRPWM of the MKV46.

What this note means?

"NOTE: FRCTRL[FRAC23_EN] should be set to 0 when the values of VAL2 and VAL3 cause the high or

low time of the PWM output to be 3 cycles or less."

Ari.

0 件の賞賛
返信
1 解決策
1,898件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Ari,

The Note says that "FRCTRL[FRAC23_EN] should be set to 0 when the values of VAL2 and VAL3 cause the high or low time of the PWM output to be 3 cycles or less.", Assume that the PWM is set up in edge alignment mode, PWMA0 pin will become high when the PWM counter reaches up to VAL2, the PWMA0 pin will become low when the PWM counter reaches up to VAL3, when the (PWMA_SMxVAL2-PWMA_SMxINIT) or (PWMA_SMxVAL1-PWMA_SMxVAL3) are equal to or less than 3, the fractional PWM function will have problem. In other words, user should select VAL2 and VAL3 register so that the (PWMA_SMxVAL2-PWMA_SMxINIT) or (PWMA_SMxVAL1-PWMA_SMxVAL3) are greater than 3 if user wants to use fractional PWM function.

Regarding the PWM example using the fractional PWM cycle, I am developing the code, I will paste here when I finish it.

BR

XiangJun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,899件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Ari,

The Note says that "FRCTRL[FRAC23_EN] should be set to 0 when the values of VAL2 and VAL3 cause the high or low time of the PWM output to be 3 cycles or less.", Assume that the PWM is set up in edge alignment mode, PWMA0 pin will become high when the PWM counter reaches up to VAL2, the PWMA0 pin will become low when the PWM counter reaches up to VAL3, when the (PWMA_SMxVAL2-PWMA_SMxINIT) or (PWMA_SMxVAL1-PWMA_SMxVAL3) are equal to or less than 3, the fractional PWM function will have problem. In other words, user should select VAL2 and VAL3 register so that the (PWMA_SMxVAL2-PWMA_SMxINIT) or (PWMA_SMxVAL1-PWMA_SMxVAL3) are greater than 3 if user wants to use fractional PWM function.

Regarding the PWM example using the fractional PWM cycle, I am developing the code, I will paste here when I finish it.

BR

XiangJun Rong

0 件の賞賛
返信
1,898件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

This is the example code for high resolution PWM developed under KDS ver3.0 and SDK version1.2, because the setting MCG is complicated, I use SDK to set up the MCG so that the KV46 can run in 100MHz.

//pls modify the system_MKV46F15.h with the following code so that the KV46 can run in 100MHz as core/system frequency, fast bus clock is 100MHz

#ifndef CLOCK_SETUP

define CLOCK_SETUP   4

#endif

BR

XiangJun Rong

0 件の賞賛
返信