HOW CAN I IMPLEMENT WIRELESS LIBRARIES ON MY KW41Z PROJECT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HOW CAN I IMPLEMENT WIRELESS LIBRARIES ON MY KW41Z PROJECT

ソリューションへジャンプ
1,685件の閲覧回数
jricaurtepino
Contributor II

Hi

I need to use the wireless libraries on my own project. i have already seen the examples and demos. I need the bluetooth libraries. Does anyone know how to do that?

 

Thanks

0 件の賞賛
返信
1 解決策
1,677件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Not the library, all the file is important. You would better develop the project based on the example.

Or you would better copy all file to your new project. 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,678件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

Not the library, all the file is important. You would better develop the project based on the example.

Or you would better copy all file to your new project. 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------