HELP, ADC of FRDM64 in differential mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HELP, ADC of FRDM64 in differential mode

ソリューションへジャンプ
1,536件の閲覧回数
hunglam
Contributor II

Hi all,

I have a problem with the ADC in differential mode. Let me explain my test settings: in order to verify the measurement of adc, I connect the internal DAC (output J4_11/DAC0 out) to the input of pin ADC0 (J4-1/ADC0_DP1) and the ground pin to the ADC0_DM1/J4-3. I program the board using kinetis design studio,  sdk 1.2/mqx standard and processor expert. The DAC works well, I have verified the output with the scope. However, the ADC also return always values ranging from 60,000 to 63,000 regardless of the DAC voltage output. The ADC is configured as followed:

16bit differential, bus clock as clock source, high speed mode, 1 extra ADCK cycle mode, no HW trigger, one-shot conversion, no DMA.

When I use the single 16bit mode, everything works just fine. But whenever I switch to the differential mode, I got the problem. PLEASE, HELP!!!!

THANKS

ラベル(2)
0 件の賞賛
返信
1 解決策
1,311件の閲覧回数
hunglam
Contributor II

I actually found the mistake. it was ridiculously stupid that it is not worth sharing it. but thanks all!

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,312件の閲覧回数
hunglam
Contributor II

I actually found the mistake. it was ridiculously stupid that it is not worth sharing it. but thanks all!

0 件の賞賛
返信
1,311件の閲覧回数
EarlOrlando
Senior Contributor II

Hello,

Could you please share your project or the code where you configure the module to reproduce the problem?

Best regards,

Earl.

0 件の賞賛
返信
1,311件の閲覧回数
mjbcswitzerland
Specialist V

Hi

When configuring for differential mode, which voltage do you have on the other signal input?

Regards

Mark

0 件の賞賛
返信