Hi all,
I have a problem with the ADC in differential mode. Let me explain my test settings: in order to verify the measurement of adc, I connect the internal DAC (output J4_11/DAC0 out) to the input of pin ADC0 (J4-1/ADC0_DP1) and the ground pin to the ADC0_DM1/J4-3. I program the board using kinetis design studio, sdk 1.2/mqx standard and processor expert. The DAC works well, I have verified the output with the scope. However, the ADC also return always values ranging from 60,000 to 63,000 regardless of the DAC voltage output. The ADC is configured as followed:
16bit differential, bus clock as clock source, high speed mode, 1 extra ADCK cycle mode, no HW trigger, one-shot conversion, no DMA.
When I use the single 16bit mode, everything works just fine. But whenever I switch to the differential mode, I got the problem. PLEASE, HELP!!!!
THANKS
解決済! 解決策の投稿を見る。
I actually found the mistake. it was ridiculously stupid that it is not worth sharing it. but thanks all!
I actually found the mistake. it was ridiculously stupid that it is not worth sharing it. but thanks all!
Hello,
Could you please share your project or the code where you configure the module to reproduce the problem?
Best regards,
Earl.
Hi
When configuring for differential mode, which voltage do you have on the other signal input?
Regards
Mark