Good low-cost debugger for Kinetis K & L-series

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Good low-cost debugger for Kinetis K & L-series

ソリューションへジャンプ
2,230件の閲覧回数
estrack
Contributor II

What's a good choice for a low-cost ($100 to $300) debugger for the Kinetis K series, that should also support the L series?

Needs to work with CodeWarrior 10.2 / 10.3


I suspect OSBDM from EBay is an option, but perhaps slow, as it is used on the tower boards (?), or CYCLONEMAX_PE, but it is $900, or perhaps PnE U-Multilink, but it has caveats as to which versions of CodeWarrior support it?


What do most of you professional devs use for debugging K series micros?

ラベル(2)
0 件の賞賛
返信
1 解決策
1,894件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

This is the CW10.3 supported tools:

tools.bmp

J-Link and USB Multilink I think are the cheaper tools.

Best Regards,

Luis

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,895件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

This is the CW10.3 supported tools:

tools.bmp

J-Link and USB Multilink I think are the cheaper tools.

Best Regards,

Luis

0 件の賞賛
返信