Getting started with TWR-K70F120

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Getting started with TWR-K70F120

1,939件の閲覧回数
juanmanuelpanie
Contributor II

hi, im writing because i have a problem with TWR-K70F120M board.

I want to probe an example project (blinky led) with codewarrior 10.6 into the board. When I debug the project with Pne U-MultiLink I get an error message: "The embedded firmware needs to be in bootloader mode to update. Please unplug the USB cable, insert a jumper on the 2-pin bootloader header (connecting JM60 IRQ to ground), and reconnect the USB cable."

I have already jumped the J10 pin but im getting the same error. I want to get in the debugger mode to download the example to the board. What am i doing wrong?

twrk70.jpg

Thank you,

Greetings from argentina

ラベル(1)
0 件の賞賛
返信
1 返信

1,722件の閲覧回数
mjbcswitzerland
Specialist V

Juan

CW10.6 is trying to update the debugger on your board (it has detected that it has an older version).

If you follow its instructions it should be able to complete this task and then you can start loading your own code to the board.

regards

Mark

0 件の賞賛
返信