Get state from PWM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Get state from PWM

1,164 Views
elisa_mejia
Contributor I

Hi,

I need to generate 7 PWMs and, simultaneously, get the states from 4 of them to update some variables. Is there any direct way to do this directly from the FTM, instead of using additional GPIO pins to detect the changes in the PWMs?

Regards,

Elisa

0 Kudos
Reply
1 Reply

1,150 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Elisa,

Port Data Input register visible in all digital pin-multiplexing modes, so please try to read the Port Data Input Register (GPIOx_PDIR).

Port Data Input register visible in all digital pin-multiplexing modes.pngPort Data Input register visible in all digital pin-multiplexing modes.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply