Generating waveforms

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generating waveforms

2,046 Views
martindusek
Contributor V

Hi,

is it possible to generate 24 MHz and 6 MHz signals (50% duty and in phase) with 12 MHz signal with shifted phase and reduced duty somehow using Kinetis microcontroller? Preferably with min. count of timer modules as we need one or two timer modules to be used for another purpose than generating this waveform?

Please see image.

Labels (2)
0 Kudos
Reply
1 Reply

1,938 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Martin,

Do you want to generate 24MHz and 6MHz signal with 12MHz signal or generate 12MHz and 6MHz signal with 24mHz signal?

If you want to generate 24MHz and 6MHz signal with 12MHz signal, it is impossible without FLL or PLL.

If you want to generate 12MHz and 6MHz signal with 24mHz signal, it is okay with FTM of Kinetis(K40/K60/K20/K10...) or eFlexPWM(KV family).

Hope it can help you

BR

Xiangjun Rong

0 Kudos
Reply