Generate a single PWM cycle in eFlexPWM without using reload interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generate a single PWM cycle in eFlexPWM without using reload interrupt

Jump to solution
2,285 Views
zorrotz
Contributor III

Hi,

In eFlexPWM peripheral, is it possible to generate a single PWM cycle, but without using the reload interrupt to finish the cycle?

 

Thanks in advance

 

0 Kudos
Reply
1 Solution
2,227 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @zorrotz,

Thanks for the clarifications. After looking into it, I have arrived at the conclusion that the only way of doing single PWM pulses is indeed by using the reload interruption.

BR,
Edwin.

View solution in original post

0 Kudos
Reply
3 Replies
2,264 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @zorrotz,

Could you please share what your part number is, as well as the SDK and IDE versions that you are using?

BR,
Edwin.

0 Kudos
Reply
2,244 Views
zorrotz
Contributor III

Hi @EdwinHz ,

My part number is MKV46F128VLL16.

The IDE version is MCUXpresso IDE v11.9.0 [Build 2144] and the SDK is 2.8.0.

 

Regards

0 Kudos
Reply
2,227 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @zorrotz,

Thanks for the clarifications. After looking into it, I have arrived at the conclusion that the only way of doing single PWM pulses is indeed by using the reload interruption.

BR,
Edwin.

0 Kudos
Reply