Gainspan GS1500M module security mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Gainspan GS1500M module security mode?

1,371 Views
danielchai
Senior Contributor I

Hi All,

I am working on the TWR-K60F120 with GS1500M tower board.

In the demo code, I enable the DEMOCFG_SECURITY to "wpa2" and set the DEMOCFG_PASSPHRASE to "123456".

But when I connect the wifi using my PC, it does not ask me for the password. PC can connect to the wifi automatically without asking for password.

Any ideas about this?

Thank you.

-Daniel

0 Kudos
Reply
2 Replies

1,274 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Daniel Chai,

      Which demo code do you modify? TWR-WiFi-GS1500M_SER2WiFi_SC?

Best regards?

Jing

0 Kudos
Reply

1,274 Views
danielchai
Senior Contributor I

Hi Jing,

Actually, I use the demo code httpsrv which is based on the MQX.

Thank you.

-Daniel

0 Kudos
Reply